Other Parts Discussed in Thread: TPS2388
Hello Community,
I ask your advice on how to properly combine chassis ground & digital ground. My doubts are related to the large number of documents that I studied and examples that I was able to obtain in the reference design library of Altium Designer boards. AN2587 http://ww1.microchip.com/...ppNotes/00002587A.pdf - Figure 7-3 shows the extent of land within a layer of land through a narrow conductor, and also indicates the required clearance between DGND & CGND. But in the examples from Altium and some documents from TI (EMI / RFI shielding - slideplayer.com/.../) a 2kV capacitor (1-4.7nF) and a 1-10MOhm resistor are used. So what is the best way to combine land? How do you think?
P.S. My application contains a set of applications such as:
- Ethernet with built-in transformer and divided grounds.
- RF antennas with a metallized housing.
- Other.
Also, my device is powered by an external network adapter from the GST series from MeanWell, but at the same time it has a metal case that contacts external metal structures that are grounded. Grounding from the housing comes to the board through the metallized holes, which are connected to the housing of the device.