This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7760: output status during fault

Part Number: ISO7760


When VCC1 of the ISO7760 is disconnected by fault event during system operation, what about the output status of ISO7760?

Regadrs,

Brian 

  • Hi Brian,

    When VCC1 of ISO7760 in un-powered for whatever reason, all the outputs on the other side will go to default/failsafe state. This is also described in Table 2 of ISO7760 datasheet listed as Function Table on page 25 under section 8.4 (also shown below). Thanks.

    Regards,

    Koteshwar Rao