This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7740: Analog Isolation

Part Number: ISO7740
Other Parts Discussed in Thread: ISO224

Dear Team,

Not sure do we have similar solution in our portfolio.

Voltage to Voltage analog isolation chip,input:0~5V output:0~5V

We need a chip which input voltage equal to output voltage. Example, input detect 1.32Vdc then output is 1.32Vdc

BR

Kevin