This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7720: Output Current

Part Number: ISO7720

What is the max current that the output can safely provide?  The data sheet specifies an absolute max of 15mA but no one wants to use this limit.  Under the recommended operating conditions it does not specify a max output current. Can the part drive 12mA without damaging the part?  Can it drive 10mA without damaging the part?

Thanks--Mark