Part Number: ISO7710-Q1
Other Parts Discussed in Thread: SN74LVC1G14-Q1,
Hi Team,
My customer is using an inverting optocoupler device in their design but has run into some issues with the input/output truth table being only valid when the power supply VDD is ready. To combat this problem, they are looking at using the ISO7710-Q1 (F-suffix version) plus an inverting buffer (SN74LVC1G14-Q1) as a functional equivalent circuit .
We'd like to run this circuit by you to make sure it won't cause any unexpected glitches that could mess up the system behavior.
The power sequencing of events is as follows:
- t=0s - 3V3D is on (3V3D also powers MCU VDDIO)
- all other power/signal should be low
- t=100ms - MCU drives SW_GPIO HIGH
- all other power/signal remain low
- t=4s - 5V_ISO is on (5V_ISO is generated by an LDO that is independent of the MCU power supply)
- expected behavior is that the output of U_1 (SW_ISO) goes from LOW to HIGH immediately because SW_GPIO is held high through out
- Question: What is the delay between VCC2 going HIGH and OUT going HIGH?
- expected behavior is for output of U_2 (SW_INV) to STAY LOW during the transition process
- SW_INV must not be allowed to "glitch" HIGH as 5V_ISO is powered on
- t=5s - MCU drives SW_GPIO LOW
- SW_ISO goes LOW
- SW_INV goes HIGH
Can you please help verify that the above sequence of behavior can be achieved in a deterministic fashion.
- Question: Are additional PU or PD resistors needed on any of the input or output pins?
Thanks,
Mitchell