This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Isolated SPI



Hi Team,

Do we have Isolated SPI like LTC6820:https://www.mouser.com/datasheet/2/609/6820fb-1271559.pdf ?

Thanks!

Yang

  • Hi Yang,

    Unfortunately, we do not have a device that is similar to LTC6820.
    If the distance between two nodes is not too far then customer can still probably be able to use ISO77xx. If the two nodes are placed farther and the datarate is <50Mbps then customer can possibly use RS-485 interface to support much longer distances. ISO14xx family has devices that support datarate from 500kbps to 50Mbps. Let us know if this is something that customer is interested in. Thanks.


    Regards,
    Koteshwar Rao