Other Parts Discussed in Thread: DRV8872, AMC1300, AMC1200, AMC1311, ISO7731
Hello,
I am using the TI DRV8872 motor driver in my design. I need to isolate the voltage across the ISEN resistor from motor ground to microcontroller ground. The datasheet for the driver says the current sense input pin voltage (ISEN) is min -0.5V and max 1V. Is there any isolation amplifier that would be suitable for this sort of application?
Thank you.