This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1540: Replace MAX14933

Part Number: ISO1540


Dear Team,

What is the suitable solution to replace MAX14933? Can I use ISO1540?

BR

Kevin

  • Hi Kuan,

    Yes, ISO1540 will be the suitable device to replace MAX14933. Please do note that MAX14933 is only available in larger 16-pin wide-body SOIC and 16-pin narrow-body SOIC packages while ISO1540 is available in much smaller, space saving 8-pin narrow-body SOIC package still supporting similar isolation ratings. Thanks.


    Regards,
    Koteshwar Rao