Part Number: ISO7810
Hello,
There is no FIT data of several device below on TI.com. Could you please provide me the FIT data and test temp(℃) of them?
| ISO7810FDWWR |
| ISO7820DWWR |
| ISO7840DWWR |
| ISO7842DWWR |
Best regards,
Yuta
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO7810
Hello,
There is no FIT data of several device below on TI.com. Could you please provide me the FIT data and test temp(℃) of them?
| ISO7810FDWWR |
| ISO7820DWWR |
| ISO7840DWWR |
| ISO7842DWWR |
Best regards,
Yuta
Hi Yuta,
Sorry about the delay. The FIT rates for the devices you requested are below:
Usage temp: 55C
| Device | FIT | MTBF |
| ISO7810FDWWR | 0.5 | 2.02E+09 |
| ISO7820DWWR | 0.5 | 2.02E+09 |
| ISO7840DWWR | 0.5 | 2.02E+09 |
| ISO7842DWWR | 0.5 | 2.02E+09 |
Best regards,
Dan