This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7710: Level translation

Part Number: ISO7710

Hi Experts,

I want to use VCC1 at 3.3V and VCC2 at 5V. In this use-case, we can translate the 3.3V signal to 5V signal.

Can we use ISO7710 like this?

Regards,

Uchikoshi

  • Hi Uchikoshi-san,

    Yes, VCC1 and VCC2 can be operated at any voltage between 2.25V and 5.5V independent of each other. Hence, applying 3.3V to VCC1 and 5V to VCC2 is absolutely fine. Please do make sure the input signal I/O logic levels match their respective VCC voltages. Thanks.

    Regards,

    Koteshwar Rao