Part Number: ISOW7841
Other Parts Discussed in Thread: ISO7841
Dear TI team:
Customer have a Ecg Project use ISO7841 ,Now there's a problem that you need to suggest.
We use creepage distance method to isolate the input and output(Similar to AC power Primary and secondary isolation). The distance between the input and output is 8mm,this way test emi Fail ,Fail frequency at 240MHZ
according to the reference design layout, test OK. But there is only FR-4 material isolation between the input and output . Customer are worried that we can not get the isolation
voltage standard, so we need a better solution