Part Number: ISO7741
Regarding to the diagram i attached below, when the ISO7741 is unpowered with VCCO, however there is a pull-up resistor connected to OUTx pin of the ISO7741 to external power supply. Is there possibly a leakage path current passed though to the VCCO of the ISO7741? and VCCO will present a voltage?