This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISOW7821: ICC max value

Genius 4860 points

Part Number: ISOW7821

Please let us know ICC max value when 3.3-V Input, and 3.3-V Output.

We found only typ value(32mA).

  • Hi Kura,

    I understand that you are looking for the maximum ICC value for 3.3V input, 3.3V output with all channels switching at 100Mbps, each output connected to CL = 15pF and with no external load on VISO pin. We usually do not characterize for this particular parameter but we expect the max ICC value to be ~60mA.

    Let me know if this is what you are looking for and if this answers your question, thanks.

    Regards,
    Koteshwar Rao