Part Number: ISO7741
We're evaluating the ISO7741F on the motor drive application.
When VCC1(Pin 1) and EN1(Pin 7) are disconnected from the 5V bias power during safety concern with motor. And at the same time, the VCC2(pin 16) and (IND)Pin11 are still connected to 5V power(in normal operation). What is the behavior with the OUTD(PIN 6)? High Z, Low or high?
Regards
Brian