Part Number: ISO7721
Dear All:
In my BMS application,the VCC pin connect the ISO7721 VCCIN ahead the GND connect the ISO7721 GND pin, Does this condition, have any effect on the ISO7721?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Big Bill,
Thank you for posting to E2E! In situations where Vcc1 is powered before GND1 is, no damage is expected if GND1 is truly disconnected. If residual charge is present or energy is coupled to GND1 such that datasheet limits are exceeded, then unexpected behavior or damage to the device could occur.
What is the voltage level of ISO7721 GND pin before GND is connected while VCCIN is powered? You are asking about the VCCIN and GND pins on the same side of an isolator as shown below, correct?
Please do expect our responses during normal business hours Monday - Friday.
Thank you, and have a great day!
Manuel Chavez