Part Number: ISO7341C
Other Parts Discussed in Thread: ISO7041, , ISO7741
Hi
Our customer is using ISO7341CDWR but wants to use VDD voltage as 1.8V.
Please check if there is a possible IC.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kim,
Unfortunately we do not have a Texas Instruments digital isolator that supports Vdd of 1.8V at the moment.
I would point out that we do have some newer digital isolators than the ISO7341C, such as the ISO7741 and ISO7041 which do have benefits such as lower power (ISO7041) and higher isolation rating (ISO7741), but neither of these support Vdd of 1.8V.
Best regards,
Dan