This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISOW7841: ISOW7841 not meeting European EMI standard?

Genius 12865 points
Part Number: ISOW7841


Hello Team,

please provide a solution to fix the 60MHz spur measured on the TI ISO7841EVM. Which common mode chokes and ferrites need to be placed? Can you provide some partnumbers, please?

See measurements below.

Thanks and Best Regards,

Hans

  • Hans,

    TDK - ACT1210-510-2P

    TSK - ACT45B-510-2P

    Wurth - 744242330

    Above are chokes that could be effective in helping with EMI. Unfortunately the EVM does not have any footprints for a choke. One would have to make some modifications to the EVM to properly solder the choke on while not compromising EMI performance. Hopefully the customer's board has footprints available for these chokes so that they can be properly placed in the layout.

    Respectfully,

    Lucas