Part Number: ISO7760
Other Parts Discussed in Thread: ISO7762, ISO7762DBQEVM, ISO7762DWEVM
Hi sir
I want to survey the ISO7760 for my new design
but I can't find the EVB, do you have any suggestion?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO7760
Other Parts Discussed in Thread: ISO7762, ISO7762DBQEVM, ISO7762DWEVM
Hi sir
I want to survey the ISO7760 for my new design
but I can't find the EVB, do you have any suggestion?
thanks
Hi Alex,
We have an evaluation module (EVM) developed for ISO776x family in both WB SOIC-16 (DW) and QSOP-16 (DBQ) packages and these EVMs come with ISO7762 soldered onto them. Since ISO7762 belongs to the same family, the performance of ISO7762 would be equally applicable to ISO7760. Alternatively, you could order ISO7762 EVM (for $49) and ISO7760 samples (for free) and replace ISO7762 device with ISO7760. The EVM should work fine without any other changes on the PCB.
Please find below the link to ISO7762DWEVM & ISO7762DBQEVM. Thanks.


Regards,
Koteshwar Rao
Alex,
You would have to buy the ISO7762 EVM and then replace the IC with the ISO7760.
Respectfully,
Lucas