This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7041: Is the sentence true? "Separated by a DOUBLE capacitive silicon dioxide (SiO2 ) insulation barrier. "

Part Number: ISO7041
Other Parts Discussed in Thread: ISO7741,

Hi team

I thought ISO7041 was double insulated like ISO7741.
However, this sentence seems to be written only on the first page.

Is it really double insulated?

best regards

Kota

  • Hi Kota,

    Yes, the ISO7041 has two isolation capacitors in series for each channel just like the ISO7741. Since there are two isolation barriers in series, it can be called as double insulated even though both of the barriers are in the same device. You can notice very similar statement in ISO7741 datasheet as well. Thanks.

    Regards,
    Koteshwar Rao