This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1042: ISOLATION FOR RS 485

Part Number: ISO1042

Hi,

Please suggest me an IC for isolation of rs485 with the creepage and the clearance to be more than 8mm and also overvolatge category 4 for less than 600vrms

The size should be as small as possilble 

isolator transceiver IC 

  • Hi Abhishek,

    The device ISO1042 that you have listed out in your post is our latest isolated CAN transceiver devices. I see that you are looking for isolated RS-485 transceiver device, for your requirement the most suitable device would be one from ISO14xx family. Please find below a table that lists out the 6 devices that ISO14xx family offers and the major differences between them (from datasheet page 4).

    The device is available in SOIC-16 (DW16) package whose creepage and clearance is slightly higher than 8mm and also supports overvoltage category IV for 600Vrms, as shown below (from datasheet page 9).

    Regards,
    Koteshwar Rao

  • thanks for replying back it suites my requirements