Part Number: ISOW7840
Hi,
I am using ISOW7840 digital isolators in a design I'm currently working on to isolate four serial streams (9600 bps) from each other, with the output conditioners for each stream fed from the isolated supply of the respective isolator. Each of these interfaces is to be shielded by compartments in the metal enclosure of the device to reduce capacitive/inductive coupling between them. Due to space constraints on the PCB, I am considering placing chassis ground traces along the centre of the isolators (along the isolation barrier) as shown in the picture below (the traces won't run under the isolator chip). Could you please advise whether this approach would affect the performance of the ISOW7840 isolators? Do you have any advise on how the shielding of the isolated interfaces should be implemented?
Thank you,
David