Other Parts Discussed in Thread: ADS124S08
Hello,
We are developing a board with the ISOW7841 that supplies two ADS124S08, and we are facing failure on radiated emission testing, as we can see below:
Our equipment has the following configuration / requirements:
- Medical equipment that must be in compliance to 60601
- Input Voltage = Output Voltage = 3.3V
- Maximum load = 100mA
- 4kVac Hipot isolation requirement
There are 6 cables of 3m length connected to the ADCs; 3 cables on each ADC.
When we unplug all cables, the emissions fall below the limit.
Could you review our current design and provide some modifications to improve these results? We can share board schematic and layout on email.
Best regards.