Part Number: ISO7641FM
We are using ISO7641 to isolate SPI signals going to low side drivers powered by field wiring. We are able to see the outputs of the ISO7641 stop functioning (not transitioning hi/low) when a radio transmitting in the UHF band ( ~ 461.5 – 468.5MHz) is brought in close proximity ( ~ 0.5m) to the device. The power is 5W. I don't know the gain of the antenna so I can't calculate field strength. We have tested this design to IEC 61000-4-3 @ 10V/m without issue so I'm assuming the field strength is much more than that.
Is there any detailed information on the frequency of the oscillator used in the ISO7641 available? We've tried different filtering methods but we suspect that the oscillator may be running at a harmonic of the radio frequency. Any guidance would be appreciated.