Part Number: ISO1500
Hello,
I have 16 ISO1500 on one PCB,my inital layout was to put each isolator and transformer above each other but this would result in a pcb length of a minimum of 10 inches.So iam thinking of putting each isolator to the left side of each isolator.First with this setup would it not be isolated?Second does laying it out this way leave it open to have problems?You can refer to the image the the aqua line area would be logic side,blue would be bus side.Would having the bus next to the logic side be a issue?Any input is appreciated thanks