Part Number: ISO7641FM
Other Parts Discussed in Thread: ADS1234, ISO7741
Hi,
The application circuit provided in the datasheet is shown in below figure.
Question 1 : The I/O level of A0, A1, SCLK and DOUT are 5v or 3.3?
Question 2 : If the I/O level (mentioned in question no 1) is 5V. If ISO7641FM providing Capacitive isolation and as well as Voltage Translator ?