Part Number: ISOW7841
Hello support team,
I have some questions about ISOW7841.
Our customer is using ISOW7841, and there is a failure that the secondary side power output (VISO) becomes 0 V in several samples.
In the customer's circuit, the decoupling capacitor on the input power supply side is 22 μF.
As a countermeasure, the customer put a bleeder resistor on the secondary output.
Nevertheless, a VISO failure has occurred.
Attach the input power and output power waveforms.
(2) After measures
In the above waveform diagrams, P5 is the primary power supply and P5C is the secondary power supply.
Are there any concerns about the cause of the failure of ISOW7841 from these waveform data?
The following points are considered.
1. When power is turned off, the primary power supply is 2.7 V or less (during lockout) and the secondary power supply is not 2.1 V or less
2. When power is turned on, the primary power supply is 2.7 V or less (at lockout), and the secondary power supply is not 2.1 V or less.
3. When power is turned on, power is turned on with a slow slope of 10 ms or more
If you have any measures to prevent ISOW7841 from malfunctioning, please let me know.
Sincerely,
M. Tachibana