This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EFT Suppressor



Hello,

 

I am Beste.

I am working at Endüstriyel Elektrik Company (R&D engineer). We produce electronic cards for industrial production and we want to protect our cards from noise and voltage deviations in industrial field. In general, we use 24V (200mA) or 220V 50-60 Hz 15Watt for electronic cards and we want to prevent instantaneous voltage distortion on all our cards.

 

Our standards are the reference;

 

IEC 61000-4-2 ESD

IEC 61000-4-4 EFT

IEC 61000-4-5 SURGE

May you please inform me about suitable filter with these standarts?

  • Hi Beste,

    Thanks for reaching out to us.
    It is best for us to make any recommendations if the noise filtering is associated with any of the TI devices so that the respective team can comment better on suggestions. I will still notify the power supply team to see if they have any suggestions.

    Could you please also confirm if you need the protection device recommendations only at the 24V input to the card? Or do you need them also at the 220V AC input? Thanks.

    Regards,
    Koteshwar Rao