Hello,
I am designing a system that requires the master module to supply 24 VDC at 3 amps to a remote module that is located in another building via a 60-metre long, single, twisted-pair (power and ground) cable. The power supply in the master module is limited to 3 amps and so this is a power-constrained application. However, the cable must be routed outside. The cable used for supplying power will be in a bundle with a Modbus cable. The system must comply with standard IEC/EN 61000-4-5 at Criteria A or B. My questions are as follows:
1. Does this application require the system to be tested using a combinational wave generator with 2 ohms of source resistance? If not, what would be the source resistance used for testing? I ask because selection of the protection devices is hugely impacted by the level and source resistance used for the test. Perhaps I missed the relevant section, but I found IEC/EN 61000-4-5 to be unclear as to whether:
i. this should be considered a direct connection to a low-power source, in part because the cable goes outside, in which case the test would require a source resistance of 2 ohms ; or
ii. it is a connection to a low-power source between power and ground, in which case the source resistance would be 12 ohms; or
iii. it is a connection to a data cable (clearly it isn't data, but there are many industrial signalling circuits require 3 amps at 24 volts) in which case the resistance would be 42 ohms.
2. Is there an advantage to shielding the power cable with the shield connected to the enclosures at both ends? If so, won't this lead to ground loops together with the protective earth?
3. Is there a reference design available for this application?
4. What devices would I use to provide adequate protection? The TVS3300 family or TVS2700 family could handle scenario 1.iii above (Ipp of about 24 amps), but at lower source resistances the value of Ipp gets very large, very fast, up to 2kA at 4kV with a 2-ohm source resistance.
Can anyone provide some clarity and/or assistance, please?
Thank you,
Peter