Part Number: ISO1050
Other Parts Discussed in Thread: ISO1042
Hi Team,
Here are a few questions about the ISO1050 that need your help:
1. Under the split termination as below shows, how can we get the value of Rterm/2 =? ,Csplit=?
2. If multiple ISO1050 CANH & CANLs are connected together as follows, then is each ISO10502 connected to a terminating resistor and capacitor (if using the split termination method)?
3. In addition, will the resistance and capacitance of the terminating resistor be affected by the number of CANs connected in parallel with ISO1050 CANH & CANL Bus?
Thanks and best regards,
Jamie