Hi Team,
My customer did ISO11452-2 test on his system and found CAN transceiver ISO1042-Q1 will stop to work then system must reset CAN transceiver to let device work. The test condition is below
ISO11452-2 Anechoic Chamber:
1 – 2GHz(CW/PM, 70V/m)
- The CAN transceiver will stop to work only on Z direction(The top side of DUT face antenna). X and Y direction work well.
- Customer's DUT work well when they change the transceiver to other vendor.
Is there any advice can help customer to pass the EMC test?
Thanks a lot.
Vincent Chen