Other Parts Discussed in Thread: ISO1211
hi
i am designing a card which reads discrete inputs with level open or ground . Please mention any IC which is having isolation.
regards
Jayalakshmi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ISO1211
hi
i am designing a card which reads discrete inputs with level open or ground . Please mention any IC which is having isolation.
regards
Jayalakshmi
Hi Jayalakshmi,
Please do share more details about your input signal to make an optimum choice. It sounded like you have a field digital input coming from a sensor that needs to be isolated and given to an MCU. Please confirm if this is the use-case. Also do share as much details as possible to suggest you a suitable device.
An example device that is meant for isolating field digital input signals is ISO1211. It doesn't read an OPEN but reads a high voltage (like 24V, 48V, 60V, etc) and 0V and provides isolated logic output to an MCU. Please do let me know if this is something similar to what you are looking for, thanks.
Regards,
Koteshwar Rao