Part Number: ISO1541
Other Parts Discussed in Thread: SN74LVC1G04, ISO7041, , SN6505B, SN6501, SN6505A
Hello, I see from the datasheet that this part uses max 4mA at 3.3V. So can this be powered from an LVC series logic gate, like a little inverter like a SN74LVC1G04 (rated at 32mA) or something similar? Or does it have higher current peaks that would require a load switch?
Also, same question for ISO7041 - since current consumption is less than 1mA can this part be powered by a logic gate, since it too has such small current?
Finally, since isolators in general can have a lot of EMI, what steps should be taken to ensure that emissions are minimized?
Thanks,
Derek