Part Number: ISO721M-EP
Other Parts Discussed in Thread: ISO721, ISO7721,
Referring to guidance in Developer's Guide: SLLA284B and datasheet SLLS629L, the recommended layer stack figure (figure 9 in SLLA284B) provided implies "no planes, traces pads or vias" should be positioned under the ISO721 on a PCB. Why is this, is this to maintain isolation between the two sides of the isolator, or to reduce EMI? This recommendation does not specify what slew/data rates this is applicable for. Please could you offer some further advice?
Considering the figure only discuses boards of 4 layers, would this still be applicable for a board with many layers? It seems unreasonable to expect all layers should be kept free of features on a many (16) layer design without an explanation of what benefit this constraint provides.
Thanks for your help,
Andy