Other Parts Discussed in Thread: ISO1044, ISO1042
Hi
I plan to let two battery packs connected in series as it shown in the below picture.
Each battery pack has the ISO1050 CAN transceiver IC inside and can communicate with the external system by CAN bus.
Each battery pack voltage is 40V. The Battery pack A is at top. The Battery pack B is at bottom.
Can I connect these two ISO1050 signals CANH and CANL directly to the external CAN bus system?
Does the signals CANH and CANL of battery pack A need to do the voltage level translation and then connect to the external CAN bus system?
If need voltage level translation, does TI have the reference design circuit?