This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How much current need to be fed to VCC1

Part Number: ISO1212


Hi,

We want to use 16 pcs ISO1212 so we need a 5V power to VCC1 of ISO1212.

How much is the output current of the power solution (Buck) for 16 pcs ISO1212 at least?

Thank you.

  • Hi Cindy,

    As stated in ISO1212 datasheet (also copied below), each unit of ISO1212 is going to consume a typical current of 1.2mA and a maximum current of 1.9mA. Hence, for 16 devices, the min current to be supported by the power supply solution should be 30.4mA. Thanks.

    Regards,
    Koteshwar Rao