Part Number: ISO7742
Hi, expert,
May I know the state of output under the condition that EN is high, power on VDD1 and VDD2, no pull-up or pull-down resistor? Is there a different between ISO7742 and ISO7742F output? Thanks.
Best Regards.
Chen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO7742
Hi, expert,
May I know the state of output under the condition that EN is high, power on VDD1 and VDD2, no pull-up or pull-down resistor? Is there a different between ISO7742 and ISO7742F output? Thanks.
Best Regards.
Chen
Hi Chen,
The suffix 'F' defines the default state of the output. Please refer to the below function table from datasheet which explains the various conditions under which the output is going to to default state. This also clarifies how ISO7742 and ISO7742F differ in function. Thanks.
Regards,
Koteshwar Rao