Hi team,
How about the output current of each channel when working at 5V and 6-ch are all at normal work?
In the POWER RATINGS part of the datasheet, it seems the maximum current is about 242mW/5.5V=44mA, but in the ABSOLUTE MAXIMUM RATINGS part of the datasheet, it seems the maximum output current is 15mA that not aligned with 15mA*6=90mA.