Part Number: ISO7041
Dear Sir, /Ms,
In the Chinese version of the webpage, there two versions for ISO7041, https://www.ti.com.cn/product/cn/ISO7041
Chinese version B: wide power supply voltage range: 2.25V to 5.5V",
English version D: updated to wide power range: 1.71 V to 1.89 V and 2.25 V to 5.5 V
I would like to confirm which will be the following versions in the future?
And according to the description of spec, it means that if the design would be worked in TA -55 ~ 125 degrees, the VCC1 & VCC2 just can be designed between 1.71V to 5.5V range.
Thank you and best regards
Rock Shao