This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7640FM: Channel -to-channel skew.

Part Number: ISO7640FM


Hello,

The ISO7640FM datasheet specifies maximum channel-to-channel skew and part-to-part skew.

Under which conditions will the part be at such maximum skews?

Can we assume these values lower under controlled temperature environments (e.g. < 30°C)?

Thanks in advance,

Rodrigo

  • Hi Rodrigo,

    These values depend on voltage, temperature and process and hence there could be a few samples that could come close to this even when only one of the three listed parameters change. By process I mean differences due to manufacturing and since this can't be avoided it is best to assume the max number even there could be a very small % parts who will come close to these max numbers. Thanks.

    Regards,
    Koteshwar Rao