Part Number: ISO7710-Q1
Other Parts Discussed in Thread: UCC28780, ISO7710
We are having no luck with ISO7710D ( by a misunderstanding - did not get ISO7710F)
Since all devices are being blown just in DC bias conditions with low frequency (100kHZ) 50% pulse, there must be something I have not understood how to use it.
See attached schematic & screenshot of placement/routing.
It is tiny PCB with GaN & controlled by UCC28780( we are far from having power yet..)
Now we measure with nothing else connected & pin 2 is lifted off the pad on the PCB. & it measures 2V.
Connecting to the driver TTL, of course, input switches 2v to 5V with the TTL getting smoking hot.
Q#1 is: since there is a 1.5Meg at the input, ok we see 2V but why would the driver at pin2 be getting hot ..is it because there is another low impedance path to pin 2?
Then what is the proper way to drive pin 2?
We are running bother at 5V & there is no visible
And also running low in parts count in the bag!
Will appreciate if you can help us shipping ISO7710FD samples by overnight shipping like good old days...5 will suffice.
-robin
ISO7710FAILURES.pptxringing at either Vcc.
Any help will be appreicated.
-robin\