Other Parts Discussed in Thread: TIDA-00555, UCC12050, ISO224, TIDA-010065, TIDA-01540
H All,
I choosed IDA-00555 reference circuit for measuring voltage (230V rms). The reference circuit used +5.0V_PH and - 5.0V_PH at the input of the AMC1100DUBR (Pg: 50/56).
I found some issues with this circuit.
1. - 5.0V_PH is mandatory must be used?
2. Pg: 51/56 The part number 750342271 (transformer) is not available as it seems to be TI customized product. Could you suggest alternate circuit to get +/- 6 Volt (isolated)