Part Number: ISO7741
There is a question about the output behavior with Input and power supply.
There are some test with ISO7741 here.
Conditions: VCC1 is floating (DC49,DC50 are not populated on the PCB)
Test 1: When INA, INB, INC are supplied by 5V,there is about 4.2V voltage can be seen between VCC1 to GND1.
Test 2: When INA is low logic,and both INB and INC are supplied by 5V,there is about 4.2V voltage can be seen between VCC1 and GND1.
Test 3: When INA and INB are low logic, and INC is high logic with 5V, the voltage between VCC1 and GND1 is continue changed in 0V to 4.2V.
Test 4: When INA and INB are low logic, and INC is low logic, there is 0V between VCC1 and GND1.
With above measurements, is this behavior normally? Could you explain why he behavior are? Very thanks.