Part Number: ISO1540
Dear Team
It seems ISO1540 will be the most suitable part to replace SI8600AD-B-IS.
Or is there any device I am not aware of?
BR
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO1540
Dear Team
It seems ISO1540 will be the most suitable part to replace SI8600AD-B-IS.
Or is there any device I am not aware of?
BR
Kevin
Hi Kevin,
Yes, ISO1540 is the most suitable device we have for I2C isolation.
Si8600AD-B-IS is 5kVrms device in WB SOIC-16 package, does customer need both 5kVrms and WB SOIC-16? We currently do not have a direct replacement device for WB SOIC-16 package. If customer does need 5kVrms, then I recommend the below solution. Thanks.
Regards,
Koteshwar Rao