Other Parts Discussed in Thread: ISO1541, ISO1540
I have a part I believe to be an I2C isolator, but I am unable to identify it from the IC markings
It is a 14 pin TSSOP and the full top face markings are:
CM077B | 55K G4 | D5PC
Thanks in advance
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi James,
Welcome to TI E2E Forum!
You can use the tool from below link to find TI product information based on package top markings. I did a quick search and found this part to be CD4077BPW which is a device with quad XNOR gate in TSSOP-14 package.
https://www.ti.com/packaging/docs/partlookup.tsp
For I2C isolation, please refer to devices ISO1540 and ISO1541. Thanks.
Regards,
Koteshwar Rao