Other Parts Discussed in Thread: ISO1541
Hello,
I need to isolation the SDI-12 Bus.
The Bus is 1 Channel bidirektional. I want to use the ISO1540 like the follow circuit.
The signal at REF1 is OK at 4,8 V.
The signal at REF2 is less than 0,5V.
I also tryit with Pullups, but it dosn´t works.
Can anybody help me, were is my mistake.
thanks
Mike