Part Number: ISO3082
Other Parts Discussed in Thread: THVD1510
Hi team,
I'm SO confused about the definition of input resistance. As you can see, in ISO3082's datasheet, it says the differential input resistance is 48kΩ. So what's the meaning of "Differential"? Does it mean that the input resistance is from bus A to bus B? I think it should be Bus A or Bus B to GND.
However, it's much more easier to understand the input resistance in THVD1510's datasheet. It's highlighted that the input impedance is bus input impedance.
So how to understand it?
Br,
Naizeng Wang