Part Number: ISO7742
Hi,
Please see the attached waveform of Isolator ISO7742.
In MCR it is used for isolation of 100Mbps RS422.
ISO_ESU is single-ended signal from transceiver to isolator measured on isolator input pin.
RXD_ESU is single-ended signal from isolator to Zynq measured on isolator output pin.
Now it is suspected the abnormal edge will lead to bit error.
Could you please give some suggestions on how to remove the step in the middle of edge?
Thanks!