Part Number: ISOW7840
We're using the ISOW7840DWER to isolate a digital signal prior to it reaching the transmitter. While it appears that we've set up the chip correctly we see that one or two bits of the 32 bit message drop low regardless of the decoupling capacitance. The design originally utilized 0.1uF caps on the VDD and V_ISO pins, however, we saw between 6 and 10 bits drop below the logic threshold. These cap values were increased to 94uF on the VDD line and 47uF on the V_ISO line and the failed bit value was decreased to 1 or 2 per message, but we still see a sudden voltage drop on the failed bits