Part Number: ISO7761
Hi Team,
My customer has questions about the output polarity that he wants to know the result of below condition.
Vcci is powered with normal voltage, say 5.0V and input signal is at high level as well. And what is the output signal polarity when Vcco voltage lies between 1.7V and 2.25V?
2. When Vcci and Vcco are powered, say 5V. If input signal 2.5V that is between 0.4xVcci and 0.6xVcci, the output signal is default, right?
Thanks a lot.
Vincent Chen