Other Parts Discussed in Thread: ESD122
Dears
Can you help recommend a Protection TVS array for usb2.0?
Thanks
Elsa Duan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ESD122
Dears
Can you help recommend a Protection TVS array for usb2.0?
Thanks
Elsa Duan
Hello Elsa,
I would recommend ESD122 to protect a USB 2.0 interface. It is a 2-channel device that has a 3.6V Vrwm, 0.2pF line capacitance, and it protects against ESD and surge events (IEC-61000-4-2 & IEC-61000-4-5).
Let me know if this device meets your needs. If so, please click the "Resolved" button.
Regards,
Matt Smith